Hi there,
i have drv8301-69m kit and a low inductance bldc motor therefore i use the proj_lab2c. The motor spins only with load, is this normal? Without load the motor turns stuttering and make strange noises, the current is about 1A. With low load the motor needs only 0.5A and i can only reach about 4A, but i know 20A should be possible. What should i change?
thanks in advance