Part Number: TMS320F28069M
Other Parts Discussed in Thread: SN65HVD257, SN65HVD33
Hi,
My project is going to get finished and I would like to have a PCB board designed based on TMSF28069M MCU. I need to have the following components on the board:
1. CAN transceiver (SN65HVD257)
2. RS485/422 transceiver (SN65HVD33)
3. PWMs
4. GPIOs
5. LEDs
My question is what components do I need to have to be able to program the PCB board through MATLAB/Simulink? Right now I'm using the Launchpad which allows me to do so but what do I need for an standalone PCB boards.
Thanks,
--Kash