This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: How to connect external memory with EMIF

Part Number: TMS320F28379D
Other Parts Discussed in Thread: TMDSCNCD28379D, LAUNCHXL-F28379D

How to connect external memory?

Is there a connector cable to be used?

What types of memories are supported?

Thanks

  • Typically, memories are included on custom PCB designs as needed.  The EMIF control and data signals are routed to the on-board memories.

    In the case of TMDSCNCD28379D and LAUNCHXL-F28379D, there is a high density connector on the PCB with access to the EMIF pins.  It should be possible to build a daughter card with external memories that interfaces through the connector.

    EMIF supports SDRAM and ASRAM memory interfaces.