Other Parts Discussed in Thread: UCC28950
Hi,
I'm designing a phase shift full bridge converter. I'm struggling with the primary transformer current reconstruction. My initial plan was to get the RMS current. But didn't take into account the Circulating current of the Ls.
So peak current is also ok. only I can't find a point to ADC sample correctly for that either.
Currently I use 1 low side current sense resistor. I'm thinking to change to a current sense transformer to reduce switching noise.
When I look into the schematics of the UCC28950 and TMDSHVPSFBKIT . They use a current transformer at the Vin+ supply. Without any additional core reset circuit. How do you prevent it from saturated at full load? I think that is a really odd please. Can you please explain?
And any suggestions how to detect if the core is saturating?
Thanks!