Hi Ti-forum,
I have another question about the uPP Modul of F28377S µC. I did a simplex communication between two microcontrollers with uPP. But I need a Duplex communication for my project.
Is the F28377S Microcontroller able to do a duplex mode?
I read the wiki-ti side. Because of this website, I thougt the µC needs other Pins with function uPP for Channel B. Or can I use normal GPIOs to feed the Channel B for Duplex-Mode?
And is it a "half" or "full" Duplex-Mode which uPP is able to do?
If the F28377s isn´t able to do a uPP-Duplex-Mode, can somone call one µC or DSP from TI which is able to do a uPP Duplex Mode.
Many Thanks in advance!!!
Best Regards,
Stefan