Part Number: TMS320F28027
Tool/software: Code Composer Studio
Dear all,
I wish to use ECAP interrupt to capture several pulse, and then change the duty cycle of PWM signal from EPWM ports. The PWM function is same as the example "Example_2802xEPwmUpDownAQ" which has about 3 interrupt already. I can use a external interrupt from keys to change the duty cycle of the PWM signal very well. However, after I add the ECAP interrupt into my program, the interrupt has never happened. I still can use the keys to change the PWM signal, but the ECAP function did not work. I learned the ECAP function from example "Example_2802xECap_Capture_Pwm". The example has only 1 interrupt, but my program has 4. The program is used to change the period of the PWM signal, but my program is used for duty cycle.
I tried to change the priority of the interrupts as the example "Example_2802xSWPrioritizedInterrupts". The problems have not really gone away.
Can some one help me please.
#define ISRS_GROUP3 (M_INT1|M_INT2|M_INT3|M_INT4) #define ISRS_GROUP4 (M_INT1|M_INT3|M_INT4) IER = 0x0000; IFR &= 0x0000; // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // This will populate the entire table, even if the interrupt // is not used in this example. This is useful for debug purposes. // The shell ISR routines are found in f2802x_DefaultIsr.c. // This function is found in f2802x_PieVect.c. InitPieVectTable(); // Interrupts that are used in this example are re-mapped to // ISR functions found within this file. EALLOW; // This is needed to write to EALLOW protected registers PieVectTable.EPWM1_INT = &epwm1_isr; PieVectTable.EPWM2_INT = &epwm2_isr; PieVectTable.EPWM3_INT = &epwm3_isr; PieVectTable.ECAP1_INT = &ecap1_isr; EDIS; // This is needed to disable write to EALLOW protected registers // Step 4. Initialize all the Device Peripherals: // This function is found in f2802x_InitPeripherals.c // InitPeripherals(); // Not required for this example // For this example, only initialize the ePWM EALLOW; SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0; EDIS; InitEPwm1Example(); InitEPwm2Example(); InitEPwm3Example(); InitECapture(); EALLOW; SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1; EDIS; // Step 5. User specific code, enable interrupts: // Copy time critical code and Flash setup code to RAM // This includes the following ISR functions: EPwm1_timer_isr(), EPwm2_timer_isr() // EPwm3_timer_isr and and InitFlash(); // The RamfuncsLoadStart, RamfuncsLoadEnd, and RamfuncsRunStart // symbols are created by the linker. memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize); // Call Flash Initialization to setup flash waitstates // This function must reside in RAM InitFlash(); // Enable CPU INT3 which is connected to EPWM1-3 INT: ECap1IntCount = 0; ECap1PassCount = 0; PieCtrlRegs.PIECTRL.bit.ENPIE = 1; PieCtrlRegs.PIEIER3.bit.INTx1 = 1; PieCtrlRegs.PIEIER3.bit.INTx2 = 1; PieCtrlRegs.PIEIER3.bit.INTx3 = 1; PieCtrlRegs.PIEIER4.bit.INTx1 = 1; // PieCtrlRegs.PIEIER3.all = 0x00FF; // PieCtrlRegs.PIEIER4.all = 0x00FF; PieCtrlRegs.PIEACK.all = (M_INT3|M_INT4); IER |= (M_INT3|M_INT4); // PieCtrlRegs.PIEIFR3.all = ISRS_GROUP3; // PieCtrlRegs.PIEIFR4.all = ISRS_GROUP4; // Enable global Interrupts and higher priority real-time debug events: EINT; // Enable Global interrupt INTM ERTM; // Enable Global realtime interrupt DBGM
ECAP function:
void InitECapture()
{
ECap1Regs.ECEINT.all = 0x0000; // Disable all capture interrupts
ECap1Regs.ECCLR.all = 0xFFFF; // Clear all CAP interrupt flags
ECap1Regs.ECCTL1.bit.CAPLDEN = 0; // Disable CAP1-CAP4 register loads
ECap1Regs.ECCTL2.bit.TSCTRSTOP = 0; // Make sure the counter is stopped
// Configure peripheral registers
ECap1Regs.ECCTL2.bit.CONT_ONESHT = 1; // One-shot
ECap1Regs.ECCTL2.bit.STOP_WRAP = 3; // Stop at 4 events
ECap1Regs.ECCTL1.bit.CAP1POL = 1; // Falling edge
ECap1Regs.ECCTL1.bit.CAP2POL = 0; // Rising edge
ECap1Regs.ECCTL1.bit.CAP3POL = 1; // Falling edge
ECap1Regs.ECCTL1.bit.CAP4POL = 0; // Rising edge
ECap1Regs.ECCTL1.bit.CTRRST1 = 1; // Difference operation
ECap1Regs.ECCTL1.bit.CTRRST2 = 1; // Difference operation
ECap1Regs.ECCTL1.bit.CTRRST3 = 1; // Difference operation
ECap1Regs.ECCTL1.bit.CTRRST4 = 1; // Difference operation
ECap1Regs.ECCTL2.bit.SYNCI_EN = 0; // Enable sync in
ECap1Regs.ECCTL2.bit.SYNCO_SEL = 0; // Pass through
ECap1Regs.ECCTL1.bit.CAPLDEN = 1; // Enable capture units
ECap1Regs.ECCTL2.bit.TSCTRSTOP = 1; // Start Counter
ECap1Regs.ECCTL2.bit.REARM = 1; // arm one-shot
ECap1Regs.ECCTL1.bit.CAPLDEN = 1; // Enable CAP1-CAP4 register loads
ECap1Regs.ECEINT.bit.CEVT4 = 1; // 4 events = interrupt
}
Four interrupt:
__interrupt void epwm1_isr(void){my code}
__interrupt void epwm2_isr(void){my code}
__interrupt void epwm3_isr(void){my code}
__interrupt void ecap1_isr(void){my code}