This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Starterware/TMS320F28335: Issue regarding flash programming of f28335 delfino control card using MATLAB Simulink

Part Number: TMS320F28335

Tool/software: Starterware

Hello,

I am using MATLAB simulink toolbox along with embedded coder for programming delfino f28335 control card. I developed a model which can receive messages from CAN (Controlled Area Network), processing it and sending back over CAN bus.

When I program in RAM (option in MATLAB as controller: delfinof 2833X)the controller works fine , but when I select for flash programming ( option in MATLAb as Controller: Delfino F2833X Boot from Flash) for working in standalone mode the controller hangs the CAN BUS and stops receiving and sending the message,  giving the CAN bus status as BUS HEAVY on CAN traffic View Manager (I am using P-CAN view).

Please guide me regarding the same.

Regards,

Vishal Savant