Other Parts Discussed in Thread: TMS320F28PLC84, TMS320F28062
Hello,
Considering the configuration: (TMS320f28PLC84 PLC modem and TMS320F28062 application MCU), I understand using the LMAC binary from the G3-DC-SDK package (www.ti.com/.../ti-plc-g3-dc) enables the nodes to function in the LMAC mode. Further, I have following three questions :-
1) Can the LMAC mode be used with multiple nodes by configuring one as TX and other nodes as RX?
I understand the message transfer can happen only if the nodes are within the transmission range, since there won't be any network formation to enable multiple hops.
2) I see there are ACKs with the LMAC mode [MAC_STAT_NO_ACK (0xE9) is one of the possible status for DATA_TRANSFER.confirm] (DC v4.8 docs: TI_plcSUITE_G3_dc_host_msg.pdf).
Is it possible to disable the ACKs ?
3) How does the addressing work in the LMAC mode. Are the messages sent in broadcast ? This would help explain in case of multiple RX nodes, how would each node respond with an ACK to the sender node ?
Any clarification would be highly appreciated.
Kind regards,
Shailja