Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: BOOSTXL-DRV8305EVM, MOTORWARE, DRV8305, CSD18540Q5B
Tool/software: Code Composer Studio
I use the launchpad-28069M and the BoostXL-DRV8305EVM board, and I run the lab05b in motorware.
Now I have a question about the DRV8305.
I can find that
ISink_LS_0p125_A = (6 << 4), //!< IDRIVEN_LS = 0.125A
in drv8305.h.
typedef enum
{
ISink_LS_0p020_A = (0 << 4), //!< IDRIVEN_LS = 0.020A
ISink_LS_0p030_A = (1 << 4), //!< IDRIVEN_LS = 0.030A
ISink_LS_0p040_A = (2 << 4), //!< IDRIVEN_LS = 0.040A
ISink_LS_0p050_A = (3 << 4), //!< IDRIVEN_LS = 0.050A
ISink_LS_0p060_A = (4 << 4), //!< IDRIVEN_LS = 0.060A
ISink_LS_0p070_A = (5 << 4), //!< IDRIVEN_LS = 0.070A
ISink_LS_0p125_A = (6 << 4), //!< IDRIVEN_LS = 0.125A
ISink_LS_0p250_A = (7 << 4), //!< IDRIVEN_LS = 0.250A
ISink_LS_0p500_A = (8 << 4), //!< IDRIVEN_LS = 0.500A
ISink_LS_0p750_A = (9 << 4), //!< IDRIVEN_LS = 0.750A
ISink_LS_1p000_A = (10 << 4), //!< IDRIVEN_LS = 1.000A
ISink_LS_1p250_A = (11 << 4) //!< IDRIVEN_LS = 1.250A
} DRV8305_CTRL06_PeakSinkCurLS_e;
but the drv8305 datasheet show that:
Please tell me which one is right ?
Thanks.