Tool/software: Code Composer Studio
Hello,
1. Can EPWM1A and EPWM1B be set up to have different frequencies, since there is one "EPwm1REG.TBPRD"?
2. Is it possible to set up 4 epwms it 1A, 1B, 2A and 3A with the following action qualifier configurations:
EPwm1Regs.AQCTLA.all = 0x0060; EPwm1Regs.AQCTLB.all = 0x0600; //for epwm1a and epwm1b
EPwm2Regs.AQCTLA.all = 0x0120; EPwm3Regs.AQCTLA.all = 0x0840; //for epwm2a and epwm3a
In short, my question here is, how do I set EPWM1B as the master.
I feel if I just use "EPwm1Regs.TBCTL.bit.SYNCOSEL = 1" there might be a conflict and ePWM1A will be used. By the way, I don't think there is anything like "EPwm1BRegs..."; so, what can be done ?
Ideas/tips will be much appreciated.
*eZdsp - F28335*