This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28335: CCS5.3 generated hex file sometimes can not be downloaded normally

Part Number: TMS320F28335


Tool/software: Code Composer Studio

Hi Ti,

I used CCS5.3 to compile the 28335 project and successfully generated the DX30_SW_S06.hex file.I use C2Prog through the serial port (SCIA)to download the program DX30_SW_S06.hex to 28335.However, in the process of downloading the program encountered a problem, as shown below。I can download the DX30_SW_S06.out file generated by the CCS synchronization via the emulator XDS200 and the program is running normally.

 

All the configuration does not make any changes, I choose another project to produce the programming file DX44_WH.hex. C2Prog can successfully download the file DX44_WH.hex.The successful download process is shown below.

Replace the download file can not be downloaded normally.Where is the problem?Project time is relatively tight, I am very anxious.