Part Number: TMS320F28377S
Hi everybody,
i have made eval board with TMS320F28377S(176 pin)(you can see part of this schematic of this boar at attached file).. so when i want to try this board, i have import some project from control suite examples and load this program to my board (without any error) then when i push to run in code composer, code composer gives below error and disconnected from board.
but when i load same program to F28377S Lauchpad of TI it runs correctly in there without any error.
i have checked everything , but i could not find the problem.
if you can help me, i will be pleasure.
C28xx_CPU1: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 6.0.628.1)
C28xx_CPU1: Unable to determine target status after 20 attempts
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging