Part Number: TMS320F2809
Looks like I'm having some issues with these pins. I'm running this chip in an industrial drives type application so I would say that it is a noisy environment. I was having a chip spontaneously reset usually after running for about 5 minutes. Sometimes it would watchdog reset, sometimes it would go into Illegal_ISR(). Looking at the design at the moment, I don't have any pull up or pull down resistors on any of those 3 pins which is different from the datasheet recommendation on page 18. Couple questions related to this:
- Can noise on these pins cause watchdog reset?
- Can noise on these pins cause Illegal_ISR()?
- Datasheet says to use pull up on EMU0 and EMU1 but it says the chip enters debug mode when EMU0 is logic high and EMU1 is logic low, so why not a pull down on EMU0 and pull up on EMU1?
- I don't need hardware debugging, can I use as low as a 0 ohm pull up/down? How about 100 ohms? I understand that I can't program like this but that doesn't matter to me.
- Would it be better to pull up to 5V instead of 3.3V?