This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049M: Further explanation of TripZone module operation

Part Number: TMS320F280049M


Hello All,

I want to ask someone who understand how the trip zone module works - in Tripzone TZCTL register you can set actions for multiple events but is there any table of priority between those events? for example if TZA is configured as force high, and DCBEVT configured as force low, there is a posibilty of conflict - how is this situation solved in the core?

Even more interesting is, that the default register value is 0 - force to high impedance state - Every bit of TZCTL register should be initialized to different value than 0 (11 - do nothing), to ensure proper operation if using only one from events?

Last question - TZCTL description table in manual contains DCBEVT2,DCBEVT1,DCAEVT1 and so on...but in TZB description we can again find DCAEVT1/2 - this means that if you set up TZA event, DCAEVT1/2 will also trigger action?

Thank you!

Miso