Other Parts Discussed in Thread: ENERGIA, TMS320F28069, TMS320F28027,
Tool/software: Code Composer Studio
I am using an energia Sketch in Code Composer Studio, I want to establish a communication by bluethoot with the launchpad, but the .cpp of the serial hardware configures the GPIO 84 and 84 for serial communication, but the launchpad does not have those physical pins.
Can anybody help me?
This is the HardwareSerial.cpp code:
*
************************************************************************
* HardwareSerial.cpp
*
* Arduino core files for C2000
* Copyright (c) 2012 Eric Ma. All right reserved.
*
*
***********************************************************************
Derived from:
HardwareSerial.cpp - Hardware serial library for Wiring
Copyright (c) 2006 Nicholas Zambetti. All right reserved.
This library is free software; you can redistribute it and/or
modify it under the terms of the GNU Lesser General Public
License as published by the Free Software Foundation; either
version 2.1 of the License, or (at your option) any later version.
This library is distributed in the hope that it will be useful,
but WITHOUT ANY WARRANTY; without even the implied warranty of
MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
Lesser General Public License for more details.
You should have received a copy of the GNU Lesser General Public
License along with this library; if not, write to the Free Software
Foundation, Inc., 51 Franklin St, Fifth Floor, Boston, MA 02110-1301 USA
Modified 23 November 2006 by David A. Mellis
Modified 28 September 2010 by Mark Sproul
*/
#include <stdlib.h>
#include <stdio.h>
#include <string.h>
#include <inttypes.h>
#include "Energia.h"
#include "wiring_private.h"
#include "sci_isr_handler.h"
#include "HardwareSerial.h"
HardwareSerial *SerialPtr;
#define SERIAL_BUFFER_SIZE 16
struct ring_buffer
{
unsigned char buffer[SERIAL_BUFFER_SIZE];
volatile unsigned int head;
volatile unsigned int tail;
};
ring_buffer rx_buffer = { { 0 }, 0, 0 };
ring_buffer tx_buffer = { { 0 }, 0, 0 };
inline void store_char(unsigned char c, ring_buffer *buffer)
{
unsigned int i = (unsigned int)(buffer->head + 1) % SERIAL_BUFFER_SIZE;
// if we should be storing the received character into the location
// just before the tail (meaning that the head would advance to the
// current location of the tail), we're about to overflow the buffer
// and so we don't write the character or advance the head.
if (i != buffer->tail) {
buffer->buffer[buffer->head] = c;
buffer->head = i;
}
}
void serialEvent();
void serialEvent() {}
void serialEventRun(void)
{
if (Serial.available()) serialEvent();
}
// Constructors ////////////////////////////////////////////////////////////////
HardwareSerial::HardwareSerial(ring_buffer *rx_buffer, ring_buffer *tx_buffer)
{
_rx_buffer = rx_buffer;
_tx_buffer = tx_buffer;
}
// Public Methods //////////////////////////////////////////////////////////////
#ifdef TMS320F28069
#define CPU_FREQ 90E6 // Set to 90 MHz for F28069
#elif defined(TMS320F28027)
#define CPU_FREQ 60E6 // Default = 60 MHz. Change to 50E6 for 50 MHz devices
#elif defined(TMS320F28377S)
#define CPU_FREQ 200E6 // Set to 200 MHz for F28377S
#else
#define CPU_FREQ 60E6 // Default = 60 MHz. Change to 50E6 for 50 MHz devices
#endif
#define LSPCLK_FREQ CPU_FREQ/4
void HardwareSerial::begin(unsigned long baud)
{
EALLOW;
#ifdef TMS320F28377S
//Configure GPIO84 as SCITXDA (Output pin)
//Configure GPIO85 as SCIRXDA (Input pin)
GpioCtrlRegs.GPCGMUX2.bit.GPIO84 = 1;
GpioCtrlRegs.GPCMUX2.bit.GPIO84 = 1;
GpioCtrlRegs.GPCGMUX2.bit.GPIO85 = 1;
GpioCtrlRegs.GPCMUX2.bit.GPIO85 = 1;
// Configure GPIO85 (SCIRXDA) as async pin
GpioCtrlRegs.GPCQSEL2.bit.GPIO85 = 3;
#else
/* Enable internal pull-up for the selected pins */
/* Disable internal pull-up for the selected output pins
to reduce power consumption. */
// Pull-ups can be enabled or disabled disabled by the user.
GpioCtrlRegs.GPAPUD.bit.GPIO28 = 0; // Enable pull-up for GPIO28 (SCIRXDA)
GpioCtrlRegs.GPAPUD.bit.GPIO29 = 1; // Disable pull-up for GPIO29 (SCITXDA)
/* Set qualification for selected pins to asynch only */
// Inputs are synchronized to SYSCLKOUT by default.
// This will select asynch (no qualification) for the selected pins.
GpioCtrlRegs.GPAQSEL2.bit.GPIO28 = 3; // Asynch input GPIO28 (SCIRXDA)
/* Configure SCI-A pins using GPIO regs*/
// This specifies which of the possible GPIO pins will be SCI functional pins.
GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 1; // Configure GPIO28 for SCIRXDA operation
GpioCtrlRegs.GPAMUX2.bit.GPIO29 = 1; // Configure GPIO29 for SCITXDA operation
#endif //TMS320F28377S
EDIS;
// ISR functions found within this file.
EALLOW; // This is needed to write to EALLOW protected registers
#ifdef TMS320F28377S
PieVectTable.SCIA_RX_INT = &uart_rx_isr;
PieVectTable.SCIA_TX_INT = &uart_tx_isr;
#else
PieVectTable.SCIRXINTA = &uart_rx_isr;
PieVectTable.SCITXINTA = &uart_tx_isr;
#endif
EDIS; // This is needed to disable write to EALLOW protected registers
// Note: Clocks were turned on to the SCIA peripheral
// in the InitSysCtrl() function
EALLOW;
#ifdef TMS320F28377S
CpuSysRegs.PCLKCR7.bit.SCI_A = 1;
ClkCfgRegs.LOSPCP.bit.LSPCLKDIV = 1;
#else
SysCtrlRegs.PCLKCR0.bit.SCIAENCLK = 1; // SCI-A
SysCtrlRegs.LOSPCP.bit.LSPCLK = 1; //LSPCLK = SYSCLK/2
#endif
EDIS;
SciaRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
SciaRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
SciaRegs.SCICTL2.all =0x0003;
SciaRegs.SCICTL2.bit.TXINTENA =1;
SciaRegs.SCICTL2.bit.RXBKINTENA =1;
#ifdef TMS320F28377S
SciaRegs.SCIHBAUD.all = (unsigned int)((F_CPU/(ClkCfgRegs.LOSPCP.bit.LSPCLKDIV * 2))/(baud*8)-1)>>8 ;
SciaRegs.SCILBAUD.all = (unsigned int)((F_CPU/(ClkCfgRegs.LOSPCP.bit.LSPCLKDIV * 2))/(baud*8)-1)&0x00FF;
#else
SciaRegs.SCIHBAUD = (unsigned int)((F_CPU/(SysCtrlRegs.LOSPCP.bit.LSPCLK * 2))/(baud*8)-1)>>8 ;
SciaRegs.SCILBAUD = (unsigned int)((F_CPU/(SysCtrlRegs.LOSPCP.bit.LSPCLK * 2))/(baud*8)-1)&0x00FF;
#endif
//SciaRegs.SCICCR.bit.LOOPBKENA =0; // Disable loop back
SciaRegs.SCIFFTX.all=0xC020;
SciaRegs.SCIFFRX.all=0x0021;
SciaRegs.SCIFFCT.all=0x0;
SciaRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
SciaRegs.SCIFFTX.bit.TXFIFORESET=1;
SciaRegs.SCIFFRX.bit.RXFIFORESET=1;
// Enable interrupts required for the sci
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block
PieCtrlRegs.PIEIER9.bit.INTx1=1; // PIE Group 9, INT1
PieCtrlRegs.PIEIER9.bit.INTx2=1; // PIE Group 9, INT2
IER |= 0x100; // Enable CPU INT
EINT;
}
void HardwareSerial::end()
{
// wait for transmission of outgoing data
while (_tx_buffer->head != _tx_buffer->tail);
_rx_buffer->head = _rx_buffer->tail;
// Disable the FIFO interrupts
SciaRegs.SCIFFTX.bit.TXFFIENA = 0;
SciaRegs.SCIFFRX.bit.RXFFIENA = 0;
}
int HardwareSerial::available(void)
{
return (unsigned int)(SERIAL_BUFFER_SIZE + _rx_buffer->head - _rx_buffer->tail) % SERIAL_BUFFER_SIZE;
}
HardwareSerial::operator bool()
{
return true;
}
int HardwareSerial::peek(void)
{
if (_rx_buffer->head == _rx_buffer->tail) {
return -1;
} else {
return _rx_buffer->buffer[_rx_buffer->tail];
}
}
int HardwareSerial::read(void)
{
// if the head isn't ahead of the tail, we don't have any characters
if (_rx_buffer->head == _rx_buffer->tail) {
return -1;
} else {
unsigned char c = _rx_buffer->buffer[_rx_buffer->tail];
_rx_buffer->tail = (unsigned int)(_rx_buffer->tail + 1) % SERIAL_BUFFER_SIZE;
return c;
}
}
void HardwareSerial::flush()
{
while (_tx_buffer->head != _tx_buffer->tail);
}
size_t HardwareSerial::write(uint8_t c)
{
unsigned int i = (_tx_buffer->head + 1) % SERIAL_BUFFER_SIZE;
// If the output buffer is full, there's nothing for it other than to
// wait for the interrupt handler to empty it a bit
// return 0 here instead?
while (i == _tx_buffer->tail);
_tx_buffer->buffer[_tx_buffer->head] = c;
_tx_buffer->head = i;
//SciaRegs.SCICTL2.bit.TXINTENA =1;
SciaRegs.SCIFFTX.bit.TXFFIENA = 1;
return 1;
}
interrupt void uart_rx_isr(void)
{
unsigned char c = SciaRegs.SCIRXBUF.all;
store_char(c, &rx_buffer);
SciaRegs.SCIFFRX.bit.RXFFOVRCLR=1; // Clear Overflow flag
SciaRegs.SCIFFRX.bit.RXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all|=0x100; // Issue PIE ack
}
interrupt void uart_tx_isr(void)
{
if (tx_buffer.head == tx_buffer.tail) {
// Buffer empty, so disable interrupts
//SciaRegs.SCICTL2.bit.TXINTENA =0;
SciaRegs.SCIFFTX.bit.TXFFIENA = 0;
SciaRegs.SCIFFTX.bit.TXFFINTCLR=1; // Clear SCI Interrupt flag
PieCtrlRegs.PIEACK.all|=0x100;
return;
}
unsigned char c = tx_buffer.buffer[tx_buffer.tail];
tx_buffer.tail = (tx_buffer.tail + 1) % SERIAL_BUFFER_SIZE;
#ifdef TMS320F28377S
SciaRegs.SCITXBUF.all = c;
#else
SciaRegs.SCITXBUF = c;
#endif
SciaRegs.SCIFFTX.bit.TXFFINTCLR=1; // Clear SCI Interrupt flag
PieCtrlRegs.PIEACK.all|=0x100; // Issue PIE ack
}
// Preinstantiate Objects //////////////////////////////////////////////////////
HardwareSerial Serial(&rx_buffer, &tx_buffer);