I debug the motor by the HFI.lib . I like to pick your brain about some HFI issues.
1: When the motor is in the HFI state, the motor makes noise. Can noise be eliminated? I should adjust which parameter to eliminate the noise.
2: When the motor is in the NS_ID state, can the phase current be adjusted? I should adjust which parameter.
3: When using the HFI, I give positive speed instructions, sometimes the motor can start forward,but sometimes the motor start reverse. IS the motor angle incorrect? I should adjust which parameter to make the motor start forward every time, when I give positive speed instructions