Part Number: TMS320F28027
Other Parts Discussed in Thread: CONTROLSUITE
Hey Gurus,
I have a question about the reading of a text file to the controller.
I would like to load the text file to the flash. For example:
Text file can read a percentage such as; 50%. under a file name of flashThis.txt, the controller would open the file and read the 50% and convert to hex and load it into one of the sectors. Using jus a simple USB stick will create the problem of the program maneuvering to the file on its own, which I would like to avoid.
I am not sure if I would be able to do this through tera term. I know I can maneuver to the file using tera term so that I know exactly what I am uploading. What is the best way for me to approach this problem.
Regards,
Rajan Joshi