This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: change Boot pin

Part Number: TMS320F28377S
Other Parts Discussed in Thread: CONTROLSUITE

 

I have successfully program z1_otpbootctrl(address 0x7810C and 0x7810D) with 0x91000B5A, and i check the value of the address 0x7810C and 0x7810D in the memory browser during under debug status. then i pull up GPIO144(0x91 - 0x01 = hex 0x90 =  dec 144) and GPIO84, connect GPIO72 to ground, but the TMS320F28377S can not run into flash code correctly, when pull up GPIO72 and GPIO84 at the same time, the flash code can run correctly.

so the user OTP new configuration for z1_bootctrl register change has no effect, i do not know why. any other setting to realize the boot pin change.

Thanks