Part Number: F28M36P63C2
Dear Friend,
I am implementing Flash Programming in F28M36 concerto controller using F021 Flash API's with M3SSCLK as 120Mhz and C28SSCLK as 120MHz.
After executing the below function i am getting status as Fapi_Error_InvalidHclkValue.
oReturnCheck = Fapi_setActiveFlashBank(Fapi_FlashBank0);
Changes i done Mentioned Here:
M3 Side:
1.Flash.c File
#if CPU_FRQ_120MHZ
HWREG(FLASH_CONFIG_BASE +
FLASHCTRL_O_FRDCNTL) = (2 << FLASHCTRL_FRDCNTL_RWAIT_S);
#endif
2.FlasProgrammingm3.c file
#if CPU_FRQ_120MHZ
oReturnCheck = Fapi_initializeAPI(F021_CPU0_BASE_ADDRESS, 100);
#endif
C28 side i also done same thing
Please guide me to resolve the problem