Part Number: TMS320F28379D
Other Parts Discussed in Thread: UNIFLASH, C2000WARE
We are working on an application that employs a number of 28379D parts, each sitting on an individual card. These cards will be tied to a master controller using a fiber-optic connection (Tx/Rx - UART). There is a need to update the firmware on these components remotely via the serial port.
The master controller has the ability to route each of the RX/TX pairs to a copper-based RS232, which can be further routed to a USB/RS232 converter. We were thinking about flashing these processors with Uniflash.
However, I do not seen a serial option in Uniflash (uniflash_sl.4.1.1329 ).
Which UART pins on 28379D have to be used to ensure compatibility with Uniflash?
Also, how do we enable the serial portion?
Thanks,
Tomas