Part Number: LAUNCHXL-F28069M
Hello,
my setup is one BLDC motor with incremental encoder and a multiturn absolute encoder. The BLDC motor drives ab big gearwheel and the absolute encoder is connected to this gearwheel.
My task is to rotate the gear between two absolute angles. In detail drive in one direction to the first angle. After this break and rotate in opposite direction to the second angle and back again.
Another similar task is to drive from angle one to angle two with a fixed speed and from two to in with higher speed, always in the same direction.
For now i’m looking for labs 13b with InstaTAC and motion planning. But it looks like InstaSpin is using relative steps with the inc. encoder. Is it possible to use the inc. encoder for the electric angle of the motor and another external absolute encoder for the position controller? The absolute encoder is connected via a CAN-BUS interface to the Evaluation Board.
Greetings,
Christian Jacobsen