This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28054M: Rs calibration problem when motor stops at mechanical endstop position

Part Number: TMS320F28054M


Hi TI and Adam,

  Rs  re-calibration can only be done when the motor is able to rotate freely at both directions during the re-calibration. (if i understand correctly)

This can create a problem when my motor has loads on it and tends on stop at my mechanical  endstop position, at this position my motor can only move freely at one direction not another.

If my motor can't move at one direction during the Rs- re calibration, the Rs re-calibration can't be done, which will cause a bigger problem when it proceeds to SPINTAC Position plan.

How do I fix this problem without increase my motor startup time? 

I have two plans to solve this problem but both of them are taking too much startup time for my motor to move

1: do the re-calibration twice if it fails at first time, which would double my startup time from 6sec to 12sec

2: use velocity plan to move my motor to a position where my motor is able to move freely at both direction before Rs-recalibration, 

Any suggestions to solve this problem effectively?