This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28377S: Can you help me to mix the code?

Part Number: TMS320F28377S

Tool/software: Code Composer Studio

I want to see the value both of temperature value and ADC value together.

I tried to mix already but it was error so, these are my codes below:

//###########################################################################
//
// FILE:   adc_soc_epwm_tempsensor_cpu01.c
//
// TITLE:  Sample temperature sensor and convert to temperature for F2837xS.
//
//! \addtogroup cpu01_example_list
//! <h1> ADC temperature sensor conversion (adc_soc_epwm_tempsensor)</h1>
//!
//! This example sets up the ePWM to periodically trigger the ADC.  The
//! ADC converts the internal connection to the temperature sensor,
//! which is then interpreted as a temperature by calling the
//! GetTemperatureC function.
//!
//! After the program runs, the memory will contain:\n
//! - \b sensorSample \b : The raw reading from the temperature sensor. \n
//! - \b sensorTemp \b : The interpretation of the sensor sample as a
//! temperature in degrees Celsius.
//!
//
//###########################################################################
// $TI Release: F2837xS Support Library v200 $
// $Release Date: Tue Jun 21 13:52:16 CDT 2016 $
// $Copyright: Copyright (C) 2014-2016 Texas Instruments Incorporated -
//             http://www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################

//
// Included Files
//
#include "F28x_Project.h"

//
// Function Prototypes
//
void ConfigureADC(void);
void ConfigureEPWM(void);
void SetupADCEpwm(void);
interrupt void adca1_isr(void);

//
// Globals
//
Uint16 sensorSample;
int16 sensorTemp;

void main(void)
{
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2837xS_SysCtrl.c file.
//
    InitSysCtrl();

//
// Step 2. Initialize GPIO:
// This example function is found in the F2837xS_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//
    InitGpio(); // Skipped for this example

//
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
    DINT;

//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2837xS_PieCtrl.c file.
//
    InitPieCtrl();

//
// Disable CPU interrupts and clear all CPU interrupt flags:
//
    IER = 0x0000;
    IFR = 0x0000;

//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example.  This is useful for debug purposes.
// The shell ISR routines are found in F2837xS_DefaultIsr.c.
// This function is found in F2837xS_PieVect.c.
//
    InitPieVectTable();

//
// Map ISR functions
//
    EALLOW;
    PieVectTable.ADCA1_INT = &adca1_isr; //function for ADCA interrupt 1
    EDIS;

//
// Configure the ADC and power it up
//
    ConfigureADC();

//
// Initialize the temperature sensor
// Note: The argument needs to change if using a VREFHI voltage other than 3.0V
//
    InitTempSensor(3.0);

//
// Configure the ePWM
//
//    ConfigureEPWM();

//
// Setup the ADC for ePWM triggered conversions on temperature sensor
//
    SetupADCEpwm();

//
// Enable global Interrupts and higher priority real-time debug events:
//
    IER |= M_INT1; //Enable group 1 interrupts
    EINT;  // Enable Global interrupt INTM
    ERTM;  // Enable Global realtime interrupt DBGM

//
// enable PIE interrupt
//
    PieCtrlRegs.PIEIER1.bit.INTx1 = 1;

//
// sync ePWM
//
  //  EALLOW;
 //   CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;
/*    do
    {
        EPwm1Regs.ETSEL.bit.SOCAEN = 1;  //enable SOCA
        EPwm1Regs.TBCTL.bit.CTRMODE = 0; //unfreeze, and enter up count mode



        asm("   ESTOP0");

    }while(1);*/
//
// start ePWM
//
  //  EPwm1Regs.ETSEL.bit.SOCAEN = 1;  //enable SOCA
  //  EPwm1Regs.TBCTL.bit.CTRMODE = 0; //unfreeze, and enter up count mode

//
// take conversions indefinitely in loop
//
   // while(1);
}

//
// ConfigureADC - Write ADC configurations and power up the ADC for both
//                ADC A and ADC B
//
void ConfigureADC(void)
{
    EALLOW;

    //
    //write configurations
    //
    AdcaRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4
    AdcSetMode(ADC_ADCA, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);

    //
    //Set pulse positions to late
    //
    AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1;

    //
    //power up the ADC
    //
    AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1;

    //
    //delay for 1ms to allow ADC time to power up
    //
    DELAY_US(1000);

    EDIS;
}

//
// ConfigureEPWM - Configure EPWM SOC and compare values
//
void ConfigureEPWM(void)
{
    EALLOW;
    //
    // Assumes ePWM clock is already enabled
    //
    EPwm1Regs.ETSEL.bit.SOCAEN    = 0;    // Disable SOC on A group
    EPwm1Regs.ETSEL.bit.SOCASEL    = 4;   // Select SOC on up-count
    EPwm1Regs.ETPS.bit.SOCAPRD = 1;       // Generate pulse on 1st event
    EPwm1Regs.CMPA.bit.CMPA = 0x0800;     // Set compare A value to 2048 counts
    EPwm1Regs.TBPRD = 0x1000;             // Set period to 4096 counts
    EPwm1Regs.TBCTL.bit.CTRMODE = 3;      // freeze counter
    EDIS;
}

//
// SetupADCEpwm - Configure ADC EPWM acquisition window and trigger
//
void SetupADCEpwm(void)
{
    Uint16 tempsensor_acqps;

    tempsensor_acqps = 139; //temperature sensor needs at least 700ns
                            //acquisition time

    //
    //Select the channels to convert and end of conversion flag
    //
    EALLOW;
    AdcaRegs.ADCSOC0CTL.bit.CHSEL = 13;  //SOC0 will convert internal
                                         //connection A13 J5:44
    AdcaRegs.ADCSOC0CTL.bit.ACQPS = tempsensor_acqps; //sample window is 100
                                                      //SYSCLK cycles
    AdcaRegs.ADCSOC0CTL.bit.TRIGSEL = 5; //trigger on ePWM1 SOCA/C
    AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 0; //end of SOC0 will set INT1 flag
    AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1;   //enable INT1 flag
    AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared
    EDIS;
}

//
// adca1_isr - Read Temperature ISR
//
interrupt void adca1_isr(void)
{
    sensorSample = AdcaResultRegs.ADCRESULT0;
    sensorTemp = GetTemperatureC(sensorSample);

    AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //clear INT1 flag
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}

//
// End of file
//

and I want to read the temperature value instead AdcaResult1 of this code below:

//###########################################################################
//
// FILE: adc_soc_software_cpu01.c
//
// TITLE: ADC software triggering for F2837xS.
//
//! \addtogroup cpu01_example_list
//! <h1> ADC SOC Software Force (adc_soc_software)</h1>
//!
//! This example converts some voltages on ADCA and ADCB based on a software
//! trigger.
//!
//! After the program runs, the memory will contain:
//!
//! - \b AdcaResult0 \b: a digital representation of the voltage on pin A0\n
//! - \b AdcaResult1 \b: a digital representation of the voltage on pin A1\n
//
//!
//! Note: The software triggers for the two ADCs happen sequentially, so the
//! two ADCs will run asynchronously.
//!
//
//###########################################################################
// $TI Release: F2837xS Support Library v200 $
// $Release Date: Tue Jun 21 13:52:16 CDT 2016 $
// $Copyright: Copyright (C) 2014-2016 Texas Instruments Incorporated -
// http://www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################

//
// Included Files
//
#include "F28x_Project.h"

//
// Function Prototypes
//
void ConfigureADC(void);
void SetupADCSoftware(void);

//
// Globals
//
Uint16 AdcaResult0;
Uint16 AdcaResult1;
//Uint16 AdcbResult0;
//Uint16 AdcbResult1;
float Voutput=0,rawValue;

void main(void)
{
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2837xS_SysCtrl.c file.
//
InitSysCtrl();

//
// Step 2. Initialize GPIO:
// This example function is found in the F2837xS_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//
InitGpio();

//
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
DINT;

//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2837xS_PieCtrl.c file.
//
InitPieCtrl();

//
// Disable CPU interrupts and clear all CPU interrupt flags:
//
IER = 0x0000;
IFR = 0x0000;

//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2837xS_DefaultIsr.c.
// This function is found in F2837xS_PieVect.c.
//
InitPieVectTable();

//
// Enable global Interrupts and higher priority real-time debug events:
//
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM

//
//Configure the ADCs and power them up
//
ConfigureADC();

//
//Setup the ADCs for software conversions
//
SetupADCSoftware();

//
//take conversions indefinitely in loop
//
do
{
//
//convert, wait for completion, and store results
//start conversions immediately via software, ADCA
//
AdcaRegs.ADCSOCFRC1.all = 0x0003; //SOC0 and SOC1

//
//start conversions immediately via software, ADCB
//
//AdcbRegs.ADCSOCFRC1.all = 0x0003; //SOC0 and SOC1

//
//wait for ADCA to complete, then acknowledge flag
//
while(AdcaRegs.ADCINTFLG.bit.ADCINT1 == 0);
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;

//
//wait for ADCB to complete, then acknowledge flag
//
// while(AdcbRegs.ADCINTFLG.bit.ADCINT1 == 0);
// AdcbRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;

//
//store results
//
AdcaResult0 = AdcaResultRegs.ADCRESULT0;
AdcaResult1 = AdcaResultRegs.ADCRESULT1;
//AdcbResult0 = AdcbResultRegs.ADCRESULT0;
//AdcbResult1 = AdcbResultRegs.ADCRESULT1;

rawValue=(float)3.0/4096;
Voutput=(float)(3.0/4096)*AdcaResult0;
//
//at this point, conversion results are stored in
//AdcaResult0, AdcaResult1, AdcbResult0, and AdcbResult1
//

//
//software breakpoint, hit run again to get updated conversions
//
//asm(" ESTOP0");

}while(1);
}

//
// ConfigureADC - Write ADC configurations and power up the ADC for both
// ADC A and ADC B
//
void ConfigureADC(void)
{
EALLOW;

//
//write configurations
//
AdcaRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4
//AdcbRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4
AdcSetMode(ADC_ADCA, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);
//AdcSetMode(ADC_ADCB, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);

//
//Set pulse positions to late
//
AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1;
//AdcbRegs.ADCCTL1.bit.INTPULSEPOS = 1;

//
//power up the ADCs
//
AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1;
//AdcbRegs.ADCCTL1.bit.ADCPWDNZ = 1;

//
//delay for 1ms to allow ADC time to power up
//
DELAY_US(1000);

EDIS;
}

//
// SetupADCSoftware - Setup ADC channels and acquisition window
//
void SetupADCSoftware(void)
{
Uint16 acqps;

//
//determine minimum acquisition window (in SYSCLKS) based on resolution
//
if(ADC_RESOLUTION_12BIT == AdcaRegs.ADCCTL2.bit.RESOLUTION)
{
acqps = 14; //75ns
}
else //resolution is 16-bit
{
acqps = 63; //320ns
}

//
//Select the channels to convert and end of conversion flag
//ADCA
//
EALLOW;
AdcaRegs.ADCSOC0CTL.bit.CHSEL = 0; //SOC0 will convert pin A0 J3:27
AdcaRegs.ADCSOC0CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCSOC1CTL.bit.CHSEL = 1; //SOC1 will convert pin A1 J3:29
AdcaRegs.ADCSOC1CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 1; //end of SOC1 will set INT1 flag
AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1; //enable INT1 flag
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared
//ADCB
/*AdcbRegs.ADCSOC0CTL.bit.CHSEL = 0; //SOC0 will convert pin B0
AdcbRegs.ADCSOC0CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcbRegs.ADCSOC1CTL.bit.CHSEL = 1; //SOC1 will convert pin B1
AdcbRegs.ADCSOC1CTL.bit.ACQPS = acqps; //sample window is acqps +
//1 SYSCLK cycles
AdcbRegs.ADCINTSEL1N2.bit.INT1SEL = 1; //end of SOC1 will set INT1 flag
AdcbRegs.ADCINTSEL1N2.bit.INT1E = 1; //enable INT1 flag
AdcbRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared*/
EDIS;
}


//
// End of file
//

Thank you in advance,

kanthanet 

  • Hello,

    Can you give me a little more detail about how the program is failing? What parts aren't working?

    I did notice that in your code above, you appear to be setting up the ADC to be triggered by the PWM, but you never change the value of CTRMODE to unfreeze the PWM.

    Whitney
  • Hello whitney,

    I just want to see the value of adc and temperature at the same time when I click play button.

    thank you in advance,
    kanthanet
  • Okay, so you're trying to modify the second code snippet you posted so that AdcaResult1 contains the temperature sensor reading and AdcaResult0 contains a sample of some other signal, correct?

    Well, you'll need add a call to InitTempSensor() like the first code snippet contains. Also note that that first code snippet configures the CHSEL field to 13 since channel A13 is connected internally to the temp sensor. You'll want to do the same in ADCSOC1CTL.CHSEL. AdcaResult1 should then contain the raw temperature sensor reading that you can then convert to degrees C using GetTemperatureC().

    Is that what you were trying to figure out?

    Whitney

  • Yes, that is my point. So, I will try to modify again with your suggestion and then I will tell you the result.

    Thank you so much,
    Kanthanet
  • Hello Whitney,

    I can do it right now

    Thank you so much,
    kanthanet