Part Number: TMS320F28377S
Hello
I'm using a F28377s.
Until now, the code was placed like all exemple with the following linker file:
BEGIN : origin = 0x80000, length = 0x000002
FLASH : origin = 0x80002, length = 0x03FFFE /* on-chip FLASH */
....
codestart : > BEGIN, PAGE = 0
.text : > FLASH, PAGE = 0, ALIGN(4)
.....
Now, for a specific need to a custom bootloader, I need to place some information before the software (Version and code length)
Then, I modify the linker file like this:
BEGIN : origin = 0x80010, length = 0x000002
FLASH : origin = 0x80012, length = 0x03FFFE /* on-chip FLASH */
....
codestart : > BEGIN, PAGE = 0
.text : > FLASH, PAGE = 0, ALIGN(4)
.....
With this, all work correctly with the JTAGdebugger, but not in standalone, the soft seems not start.
What is my mistake?
Thank