This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027: Flash and EMUPower

Part Number: TMS320F28027


Hello Gurus, 

I had a question about the EMUpower. 

Currently I am able to load the code onto  the controller.

What I notice is very peculiar:

1. Upon cycling the power it does not start the code (USB cable not plugged from controller to PC)

2. Leave USB cable plugged in, cycle power, same result the code does not start. 

What does work :

1. After flashing, remove the USB, cycle power and then plug in the USB cable. ( I can unplug it too and it works)

I notice that the EMUPower LED turns on and the code starts running as it should. 

I would like to run my code without the USB cable attached. So that upon cycling the power my code will start running. 

What is the connection between the USB/EMUPower LED and the Program running from flash?

Regards,

Rajan Joshi