Other Parts Discussed in Thread: DRV8301
Hello -
I have custom hardware and have done quite a bit of real-world testing on it. It has worked quite well.
I've been using mostly speed control, and have now disabled the controller and am using torque control (commanding IqRef_A). Controller starts up fine, responds to my throttle inputs. However, once spinning at a decent speed, when I command an IqRef_A of 0.0, the motor continues to spin, and may even continue to accelerate... If I apply a sufficient load to the motor, this does not seem to happen. But with a light load or no load, this phenomenon occurs.
Any obvious things to check? This is currently a major issue for me.
Any help is much appreciated!
Best,
-asifjahmed