Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: MOTORWARE
Tool/software: Code Composer Studio
I'm using the InstaSpin lab 5a as the base of my project, and I would like to export all the files that it uses into a folder. I would like to separate it out, so that I can track my code with Git and share it as an open source project. There are no code files in the project folder and everything is dispersed throughout a web of folders in Motorware. I think it would be nearly impossible to identify each file and put it in a separate folder by hand.
This shouldn't affect the question much, but I'm doing development with a Launchpad-F28069M and the Boosterpack-drv8305.
If this is the wrong way of going about it, please suggest a better way to keep track of the code. But I think separating it out is the best option, because there are a lot of files that need to be modified for each specific application, like adding sci bus functionality.
My version of CCS is 7.1.0.00016