Part Number: F28M35H52C
We are using F28M35H52C for the board. In this we are able to boot the device with serial interface.
When we make it run (blinky.c) it is not running and rather it is generating XRS Pin low for around 25us (we have 20M oscillator on board) @ 915 Hz frequency.Also, we have checked the BOOT Pins and these are high when XRS pin is low. Also, when connecting JTAG, i am getting "No source available for 0x1001692".
we have used same controller previos project also. If a load same project in new board then also it's XRS Pin is toggling.
Re,
Umang