Hello TI
Any update regarding this issue with Windows 10? I am facing the similar issue with TMS320F28069UPFPS USB CDC and DFU class drivers (composite device). We are using these drivers for Windows 7 from more than a year. But while connecting same device with Windows 10 PC, the PC is not recognizing it as a specific device instead acting as Windows native device (as mentioned earlier). Even though I am installing the specific drivers manually, but it is not communicating with our device as expected. I have also attached the code trace log for failure message.
Here I am attaching the code-trace log: Error message - Can't read language table.
This issue is quite critical for us as we are moving for production. Also I do not have much experience with USB and Windows drivers. So please let me know if any further information is required.
Thanks in advance