Hi all,
Little confustion in page no:2243 in TRM on MSG_NUM field. Please find the description below.
The Message RAM supports maximum 32 Message objects, using the MSG_NUM fileld 32 different message values can be assigned to the Message object in the range 0x01 to 0x80 as specified below, Is it correct???
*****************************************************************************************************************************
7-0 MSG_NUM R/W 1h Number of message object in Message RAM which is used for data transfer
0x00 Invalid message number
0x01-0x80 Valid message numbers
0x81-0xFF Invalid message numbers
Note: This bit is write protected by Busy bit.
Reset type: SYSRSn
*****************************************************************************************************************************
Page no 2182, FIGURE 22-1 CAN Block diagram has blocks with colors like blue, green etc. some are with same, what are significations of colors??
Thanks