Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
Hi,
I am using a 28377S Launchpad to get code working for the Buffered DAC A Output pin on the Launchpad / Processor. Right now I am scoping Launchpad pin 27 and I am seeing some weird behavior with clipping of the DAC output.
First of all, I have working code which changes the DACVALA field in the DacaRegs Register (checked by looking at the register values through the JTAG header on the launchpad). I am cycling between 20 and 4020 bits on the register with a 1/2 Hz sine wave, which should correspond to ~0 to 2.9 Volts on the Launchpad. However, I get the following results on the scope. The lower end of the Sine wave is clearly visible, but the upper end (above 700mV is saturating). I am literally using nothing except for a 28377S Launchpad.
First, is there some reason I am not considering that the DAC A output would be saturating on the processor?
Second, is there an issue with the launchpad 28377S hardware?
I have tried switching between the VREFHI at 3V on the Launchpad and an external VDAC reference, it does not change the results of this. Any ideas?