Hi,
I have used the interrupt for SCI (SCITXINTA) which is y = 9, x = 2, and it works fine.
Now I want to change the priority of SCITXINTA. Then I changed the definition in library file "F2806x_SWPrioritizedIsrLevels.h" as follows:
As You can see, INT9PL is changed to 0, which means not used. But the SCI sends back response during communication. I am confused.
Best regards,
WL