This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: serial flash programming at SCI Boot mode

Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE

Hi,

I try to flash programming using serial flash programmer at SCI boot mode.

I turn off the board and set the boot mode. ( GPIO72 : 0, GPIO84 : 1)

and turn on the board.

The program 'serial_flash_programmer.exe', provided by TI, was used to perform the following steps, but the process is no longer in progress.

The situation is as bellow.

I do not know why it is not progressing anymore.

Please help me.