This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049M: F280049PM difference in Q100PM and PM

Part Number: TMS320F280049M


Hi Champion,

I find in F280049 Datasheet, F280049PM package has two type, one is Q100, another is regulat PM, I check the pin difference, Q100 package remove GPIO12, 13m chage to Flt1, FLT2.

So expect the Q certification and GPIO difference, is there any other change in Q version PM package?

If my customer want to use it in auto application, they should reference Q vsrion pin map to layout, right?

All F28004X family will have different pin map in PM package Q and non-Q version?

Is otner package lik PZ also has pin difference between Q and non Q?

Thanks!

BR

Joe