Part Number: TMS320F28375D
Dear,
What is significant of below bit for TMS320F28375D?
Flash0CtrlRegs.FBAC.bit.VREADST
in older example code this is not available where in new example code this is available in "void InitFlash(void)".
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28375D
Dear,
What is significant of below bit for TMS320F28375D?
Flash0CtrlRegs.FBAC.bit.VREADST
in older example code this is not available where in new example code this is available in "void InitFlash(void)".
Amtech,
Please read the section 2.12.6 Flash and OTP Power-Down Modes and Wakeup in TRM at 
In this section, procedure to enter Flash low power mode is explained. As mentioned in that procedure, VREADST should be configured before powering down the Flash to ensure the requisite delay needed for the flash pump/bank to come out of low-power mode.
Thanks and regards,
Vamsi