Part Number: TMS320F28069M
Tool/software: Code Composer Studio
Hello,
I'm trying to create a project with HAL from the scratch, but I'm getting a list of unresolved symbols - ex. _EST_getFlux_pu referenced in ./user.obj. When comparing my project with the example (proj_lab01) I see that those symbols exist in a library called "2806xrevb_fastspinromsymbols.lib" included in the example.
I cannot find any information about this library, what is it for? Does it somehow substitute additional source files that would define the unresolved symbol (ex. from EST module)?
Anyways - when I add this library to my project, I get a list of errors #16008, which means that the library was compiled for different ISA version (C2800). The error says that C2700 was specified in a previous file or on the command line. I cannot find it, where might it be specified? As for RTS I've chosen "rts2800_fpu32.lib".