I have a question. It is from my customers.
1. For the data retention duration time of the built-in flash ROM of the TMS320F28023, is the retention period shown below even when VDDA, VDD and VDDIO are being supplied?
When Tj = 125 ° C, 0.4 years
When Tj = 100 ° C, 1.5 years
When Tj = 55 ℃, 29.6 years
※ For general power generation applications, Ta = 70 ℃ is common. Calculating the above retention period by the Arrhenius rule, if Tj = 70 ° C is exceeded, 10 years can not be guaranteed.
2. Please tell us about the TI products that are guaranteed 105 ° C 10 years in general specifications for automotive and industrial applications.
3. We are planning to conclude NDA. Still can not you teach detailed data and conditions?