This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027: SCI print int

Part Number: TMS320F28027


Hello Gurus, 

I would like to print something that I have stored in flash to tera term using SCI. 

I am trying to use the scia_xmit as my print, but it returns an ascii. 

Do i have to convert this into an int and send it one character at a time ?

Is there no way to send the integer directly? 

For example if I store the value of 100 in flash which is 64 in hex, I can read the flash and then when i print the int, it will print d (100 in ascii).

I would like to print the value of 100 on the screen. 

How should i proceed?

Regards,

Rajan Joshi