Part Number: DRV8301-69M-KIT
Tool/software: Starterware
I plugged in a sensorless brushless motor to the board and tried to identify the motor.
The first time the identification is OK.
But when I tried to identify it later, it is just stuck at 0% percent, and at the F28069 side, two leds turned red.. I reinstalled the software, nothing changed.