Hi
I need an urgent support regarding the F28035 piccolo link file and load .out file.
I can not continue with the project because of this problem.
I load the out file from the "F28xx on chip flash programmer" in the CC but the program is not running..
The program stuck on an outside memory area or on "_DSP28x_usDelay" function - without running!
I use the "F28035_CLA_lnk.cmd" link file because Im using the CLA + CPU memory.
Please advice what to do,