Other Parts Discussed in Thread: CONTROLSUITE
Hi, as i said in past posts i am working with a Lauch F28069 recently and im having some weird problems. i am developing a power inverter with a sinusoidal patter of commutation, in the code i need to include the math.h file. but when im using the sin function, it gives me values that not correspond with the sin function. i thought it could be a problem with the source code of the library, but then i tested de function in a F28027 that i was working before and there the sin function works perfeclty and the values offered by this are correct. why is that? i might have to do another configuration? there is any explanation for this? (lately almost of all of my problems are because im missing some flash configuration).
All helps are welcome. Regards.
Eliomar Conde.