Hello
Currently, I have a project in GUI Composer v2 for my microcontroller. My target communication setting is set to XDS, and I have a target program set that I wrote in CCS v6.2. From the target communication settings, I have tested the connection and GUI Composer shows that everything connects fine. When I attempt to run my program, it does not always run. In fact, i'd say it runs half the time I try to run my program. If it doesn't work, I typically press the reset button on my microcontroller or run my program through CCS first, then I try to run my program from GUI composer and usually it works. Today GUI Composer hardly worked at all. My graph would populate at first, and then it wouldn't update and I wasn't able to interact with my interface. Even when I download the program as a stand alone app, it works sometimes. Can anyone explain this?
If this makes a difference, I did have to delete a .gel file located in the following directory due to the fact that my project had a RAM Build Configuration.
<your user folder>\AppData\Local\Texas Instruments\TICloudAgent\loaders\ccs_base\emulation\gel
Thank You