This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069M: Inertia Identification failed

Part Number: TMS320F28069M
Other Parts Discussed in Thread: DRV8301-69M-KIT, MOTORWARE

Hi all,

I fail to identify the inertia every time.

Error 2004 or 2006 is output when identifying inertia.

Then, we reduced the values of “gMotorVars.SpinTAC.VelIdGoalSpeed_krpm” and “gMotorVars.SpinTAC.VelIdTorqueRampTime_sec”,

and finally set them to "1". However, the same error is still output.

Please advise what is the problem.

HW environment

  • Board : DRV8301-69M-KIT
  • Motor : Original motor
    • R : 5.25Ω
    • L : 10mH
    • FLUX : 2.45
    • Pole pairs : 10
    • Max motor speed : 600RPM 
    • Max motor current : 4.8A
    • Inertia : TBD

SW environment

  • motorware_1_01_00_17 : lab5e

I am using "motorware_selecting_user_variables.xlsx" to set the parameters of "user.h".

Best regards,

Sasaki