This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

what is possible to do with drv8312-69m-kit

Hi there,

I am currently working on my Bachelor thesis with the topic "Analysis of dynamic processes on a BLDC". Now I would like to know if it is possible to start the BLDC with different input sizes. I want to investigate motor run-ups with diffent frequencies (50Hz, 60Hz,  ...), is this possible? And I want to know, if it's possible to make a graphic with diffent variables ( Current, torque, speed, frequency,...)while the motor is running?

It's hard for me to understand the documents because of the language, so I hope someone can help me.

I'm using the drv8312-69m-kit with the BLDC.

Thanks and best regards