Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
I was trying to load the example program "sci_loopback_interrupts" in the flash memory of TMS320F28379D to make it work standalone. For that I selected the "Flash" as the active configuration and "2837x_FLASH_lnk_cpu1.cmd" as the linker command file. But still I am getting 93 errors while building the project. How can I solve this problem? Do I have to make any changes in the "main code"? If yes, how can I do that? Is there any available manual to learn this ? I want to add that I am using "ccs 7.1.0 " version and "control suite 3.4.1" version.
Mohammad Arifur Rahman