Part Number: TMS320F28377S
Tool/software: Code Composer Studio
Hello,
I am unable to program 28377S on a custom board.
I am using an XDS100 JTAG adapter and Code Composer Studio 6.
The following error is displayed:
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 6.0.628.1)
C28xx_CPU1: Unable to determine target status after 20 attempts
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
I've verified +3.3V and +1.2V supply voltages to the chip, and the XRS pin..
Any suggestions where to look next?