This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

sensorless BLDC motor controller

Other Parts Discussed in Thread: BOOSTXL-DRV8301, CONTROLSUITE

Hello

I have a sensorless  brushless DC motor ( T- motor--AT 2820) with this specifications:

I want to control the motor speed from 10 rpm to 8000 rpm

I used a 30 A fly fun speed controller, for driving, an optical encoder to read the speed and PID controller with TM4C1231H6PZIR.  but the start up speed was 400 rpm, It's important for me to control the speed at low speed (~10rpm). Is the DRV8301-HC-C2_KIT or BOOSTXL-DRV8301 suitable for this application?

Regards