Other Parts Discussed in Thread: SFRA
Tool/software: Code Composer Studio
Hello,
I am new to Code Composer and am following the examples in C2000 Digital Power BoosterPack User's Manual. In the first example for Buck_VMC_F2837xS open loop control, when you are supposed to use the SFRA tool, it states " Set Active_LD1_EN to 1 in the expressions window. Also set Continuous_ON to 1". However this causes an over-current trip and the FaultFlg1 changes from zero to 1. I try clearing the fault and setting the duty cycle to 0.3 as was done before but the over-current trip will not go away. This is the output from SFRA which does not match what's shown in the example. Has anyone gone through the examples in the User's Manual and experienced this? I am only able to set the duty cycle back to 0.3 by setting Active_LD1_EN and Continuous_ON back to zero as it originally was.