Hi,
I was wondering if we can have a combined trigger source for any ADC.
I know that one of the CPU timers or ePWM SOCs can be used as trigger source. But, in one of the application, I would like to measure some 20 samples using CPU 1 clock which has period of 250ns. But this process has to be started at the start of ePWM1 which has period of 11.7 us (85 KHz). So, once the capturing starts at the start of ePWM, I would like to continue measuring using CPU1 clock. The next set of values should follow the same process ie, start the process at the start of ePWM1 and continue measuring at CPU1 clock.
Is there any way to combine the the trigger sources?