Other Parts Discussed in Thread: BOOSTXL-DRV8305EVM
HI,
My kit is C2000 piccolo Launch PAD (LAUNCHXL-F28027F) with BOOSTXL-DRV8305EVM and I have been trying to run the motor using externally saved (in a separate flash) calibration Data. Idea is to not to start calibration of the motor but to run using those pre-calibrated saved values. I can read the motor parameters to the program and set Rr_ohm, Rs_ohm, Lsd_H, Lsq_H, and Flux_VpHz in gMotorVars to the values I wanted. After that I did the following flag settings:
gMotorVars.Flag_enableSys = true; gMotorVars.Flag_Run_Identify = false; gMotorVars.Flag_MotorIdentified=true
However, once it done all the motor parameters were cleared and cannot load to the values I need. Could you please tell me what steps/ other flag settings that I need to perform in order to get the motor in REAL identified state?
Thank you very much!